DOCA0239EN-11

Software Requirements

The TeSys island DTM Library requires the following software installed on the PC:

  • Microsoft .NET Framework v3.5 SP1

  • EcoStruxure Control Expert v15.0 SP1 or later, EcoStruxure Machine Expert v1.2.7 or later, SoMove software v2.9.7 or later

  • Modbus DTM Library v2.6.12 or later

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?