DOCA0239EN-11

Installation Preparation

The execution of setup file of the TeSys island DTM Library will extract the appropriate set of files on the local hard drive. The installation of the DTM library starts automatically.

Before starting the installation, perform the below steps:

  • Close the DTM applications running on the PC before starting the setup program.

  • Log in with the user ID having administrator or equivalent role to install the TeSys island DTM Library.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?