DOCA0239EN-11

Version 2.4.4

Bugs Fixed

If there are more than 15 avatars configured or the total number of avatar input dataset in TeSys island exceeds 250 bytes, then IO scanning will not perform in EcoStruxure Control Expert (ESCE).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?