DOCA0239EN-11

Installation Directories

Once the TeSys island DTM setup files are downloaded, the files are installed in the Program Files folder by default.

Supported Operating System

Folder

64 Bit

C:\Program Files (x86)\Common Files\Schneider Electric Shared\Schneider Electric TeSys island DTM Library

32 Bit

C:\Program Files\Common Files\Schneider Electric Shared\Schneider Electric TeSys island DTM Library

The setup files folder will consist of dll and configuration files.

If you are upgrading the setup files from the previous release of the software, the previous version setup files are overwritten by the new version files in the Program Files folder.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?