Quick Start Guide
Overview of the Application Example
Introduction
The Quick Start Guide uses an application example to illustrate each step in the process of installing, configuring and using TeSys T.
The application example uses the LTM R controller to protect and control a motor and its driven load, in this case, a pump.
This application example is intended to:
-
show you how to configure the LTM R controller in a few steps,
-
provide an example you can modify to develop your own configuration,
-
serve as a starting point for the development of more complex configurations, incorporating such additional features as HMI or network control.
Functions Performed
When the LTM R controller has been configured in order to protect and control the motor and pump, it will perform the following functions:
-
thermal overload protection
-
motor temperature sensor protection
-
voltage protection / undervoltage
-
external ground current trip protection
-
initial system configuration during commissioning using PC and SoMove software
Operating Conditions
The operating conditions used in the application example are:
-
motor power: 4 kW
-
line-to-line voltage: 400 Vac
-
current: 9 A
-
control circuit voltage: 230 Vac
-
3-wire control
-
motor trip class 10
-
start button
-
stop button
-
reset button on enclosure door
-
trip light
-
alarm light
-
full voltage, non-reversing starter (direct over the line starter)
-
24 Vdc power supply in the motor control center or control station for future use with LTM E expansion module inputs
Network Conditions
The network conditions for the example are:
-
protocol: DeviceNet
-
address: 1
-
baud rate: Autobaud
The LTM R controller is configured via SoMove, not via the network (configuration via network port is disabled).
The network software setup described in this document uses RSNetWorx configuration software for network configuration and Studio 5000 for PLC configuration.
Components Used
The application example uses the following components:
Item |
Component Description |
Reference Number |
---|---|---|
1 |
LTM R 100-240 Vac DeviceNet motor management controller (1.35...27 A FLC) |
LTMR27DFM |
2 |
LTM E 100-240 Vac expansion module |
LTMEV40FM |
3 |
LTM R to LTM E RJ45 connection cable |
LTMCC004 |
4 |
USB to RS485 converter |
TCSMCNAM3M002P |
5 |
SoMove software version ≥ 2.3 |
SoMove |
6 |
TeSys DTM Library v2.8 for TeSys T and TeSys U |
DTM Files |
7 |
External ground current trip CT |
TA30 |
8 |
External PTC binary motor temperature sensor |
User supplied |
Presentation of the TeSys T Motor Management System
System Overview
The TeSys T Motor Management System offers protection, control, and monitoring capabilities for single-phase and 3-phase AC induction motors.
The system offers diagnostic and statistics functions and configurable alarms and trips, allowing better prediction of component maintenance, and provides data to continuously improve the entire system.
The 2 main hardware components of the system are:
-
the LTM R controller, and
-
the LTM E expansion module.
System Presentation
The following tables describe the main components of the TeSys® T Motor Management System.
LTM R Controller |
Functional Description |
Reference Number |
---|---|---|
|
LTMR08DBD (24 Vdc, 0.4...8 A FLC) |
|
LTMR27DBD (24 Vdc, 1.35...27 A FLC) |
||
LTMR100DBD (24 Vdc, 5...100 A FLC) |
||
LTMR08DFM (100...240 Vac, 0.4...8 A FLC) |
||
LTMR27DFM (100...240 Vac, 1.35...27 A FLC) |
||
LTMR100DFM (100...240 Vac, 5...100 A FLC) |
LTM E Expansion Module |
Functional Description |
Reference Number |
---|---|---|
Additional components required for an optional expansion module:
|
LTMEV40BD (24 Vdc logic inputs) |
|
LTMEV40FM (100...240 Vac logic inputs) |
SoMove Software |
Functional Description |
Reference Number |
---|---|---|
Additional components required for SoMove software:
|
SoMove ≥ 2.3 |
|
TCSMCNAM3M002P (USB to RS485 converter) |
LTMCU Control Operator Unit |
Functional Description |
Reference Number |
---|---|---|
Additional components required for an optional HMI device:
|
LTMCU |
|
LTM9CU30 (HMI communication cable) |
||
TCSMCNAM3M002P (USB to RS485 converter) |
||
LTM9KCU Kit for portable LTMCU |
LTM R and LTM E Description
The following diagrams show the features of the LTM R controller and LTM E expansion module:
Installation
Overview
The following procedure describes how to install and physically configure the TeSys T system, according to the operating conditions used in the application example. The same procedure is used for other configurations.
The full installation procedure is shown on the Instruction sheets provided with the LTM R controller and the LTM E expansion module. It is also described in detail in the Installation chapter of the User Manual.
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Turn off all power supplying this equipment before working
on it.
Apply appropriate personal protective equipment
(PPE) and follow safe electrical work practises.
Failure to follow these instructions will result in death or serious injury.
|
The following diagrams show the physical dimensions of the LTM R controller and the LTM E expansion module:
Mount LTM R and LTM E
Mount the LTM R controller and the LTM E expansion module, respecting clearance zones and operating position.
Connect LTM R to LTM E
Connect the LTM R controller and the LTM E expansion module using the RJ45 cable.
Connect to a TeSys T LTMCU HMI Device (Optional)
Wire Current Transformers
Wire the current transformers according to the operating conditions:
-
Product range → 1.35...27 A
-
Nominal motor current → 9 A
Wire Ground Current Sensor
Wire LTM R
-
Wire the power supply and the I/O.
-
Wire the temperature sensors.
NOTICE |
---|
LOGIC INPUTS DESTRUCTION HAZARD
Failure to follow these instructions can result in equipment damage.
|
Wire LTM E
The 4 logic inputs on the LTM E expansion module (I.7 - I.10) are not powered by the control voltage of the LTM R controller.
Wire the voltage transformers and the I/O on the LTM E expansion module.
Use of AC Interposing Relays
The use of an AC interposing relay is allowed only on short distances if an AC voltage is mandatory.
AC RSB1 relay voltage |
24 VAC |
48 VAC |
120 VAC |
230/240 VAC |
Maximum distance for wires in parallel without metallic screening |
3,000 m (10,000 ft) |
1,650 m (5,500 ft) |
170 m (550 ft) |
50 m (165 ft) |
Maximum distance for wires in parallel with metallic screening |
2,620 m (8,600 ft) |
930 m (3,000 ft) |
96 m (315 ft) |
30 m (100 ft) |
Use of AC Interposing Relays with a Rectifier
The use of AC interposing relay with a rectifier is recommended on long distances if an AC voltage is mandatory.
Add a rectifier composed of 1 A / 1000 V diodes to command an AC interposing relay. In this way, rectified AC current flows in the control cable when the switch in the continuous part is closed.
AC RSB1 relay voltage |
24 VAC |
48 VAC |
120 VAC |
230/240 VAC |
Maximum distance for wires in parallel without metallic screening |
3,000 m (10,000 ft) |
3,000 m (10,000 ft) |
3,000 m (10,000 ft) |
3,000 m (10,000 ft) |
Maximum distance for wires in parallel with metallic screening |
3,000 m (10,000 ft) |
3,000 m (10,000 ft) |
3,000 m (10,000 ft) |
3,000 m (10,000 ft) |
LTM R Controller Wiring
The diagram below illustrates the main power circuit and the 3-wire (impulse) local control with network control selectable, corresponding to the application example.

1 Contactor
2 Ground current trip transformer
3 PTC binary thermistor
4 Detected alarm indication
5 Detected trip indication
L Local control
O Off
N Network control
Configuration
Overview
After the wiring connections are made, the next step is to configure parameters using SoMove software (see the SoMove chapter of the User Manual for more details).
![]() |
---|
UNINTENDED EQUIPMENT OPERATION
The application of this product requires expertise in
the design and programming of control systems. Only persons with such
expertise should be allowed to program and apply this product.
Follow all local and national safety codes and
standards.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Connect to SoMove™ Software
Set Parameters
Step |
Action |
Result |
---|---|---|
1 |
Start the software. |
– |
2 |
In the screen, select the button on the left side. |
The dialog box opens. |
3 |
Select the button in the upper-right corner of the window. |
dialog box opens. |
4 |
In the dialogue box, make the following settings:
|
|
5 |
Confirm the selected setting and click . |
The dialog box appears. |
6 |
In the dialog box, select the button.NOTE: The SoMove software will search for any TeSys T that is
connected through the USB to RS485 converter cable.
|
The TeSys T unit will appear in the blank space above the button. |
7 |
Once the TeSys T unit appears, click . |
The screen appears. |
8 |
Select the button. |
The dialog box opens. |
9 |
In the dialog box, make the following selections:
|
|
10 |
Confirm the selected settings and click . |
The dialog box opens. |
11 |
In the dialog box, select the controller, controller firmware version, expansion module, and expansion module firmware version. For this example, the following settings were selected.
|
|
12 |
Confirm the selected setting and click . |
The SoMove project landing page opens. |
13 |
Select the List of Parameter Settings. tab to set up the TeSys T device. The example application parameters are set up per |
– |
14 |
Select to save the configuration file. |
The dialog box opens. |
15 |
Enter a relevant name and click . |
– |
List of Parameter Settings
Parameter settings for the application example:
Device Information Branch |
Sub-branch |
Parameter |
Setting |
---|---|---|---|
Device information |
– |
Current range |
1.35-27 A |
Network |
DeviceNet |
||
Control voltage |
100-240 Vac |
Settings Branch |
Sub-branch |
Parameter |
Setting |
---|---|---|---|
Motor and Control Settings |
Motor operating mode |
Nominal voltage |
400 V |
Nominal power |
4 kW |
||
Operating mode |
3 wire independent |
||
Contactor rating |
9 A |
||
Phase |
3 phase |
||
Motor temperature sensor |
Sensor type |
PTC binary |
|
Trip enable |
Enable |
||
Trip level |
According to motor |
||
Alarm level |
According to motor |
||
Load CT |
Load CT ratio |
Internal |
|
Load CT passes |
1(1) |
||
Ground Current Sensor |
Ground Current Sensor ratio |
1000:1 |
|
Control mode |
Local control |
Terminal trip |
|
Thermal Settings |
Thermal overload |
Trip type |
Inverse thermal |
Trip class |
10 |
||
FLC1 (1) |
50 %(1) (equivalent to 9 A) |
||
Trip enable |
Enable |
||
Alarm enable |
Enable |
||
Current Settings |
Ground Current Mode |
Trip enable |
Enable |
Trip level |
1 A |
||
Trip timeout |
0.5 s |
||
Alarm enable |
Enable |
||
Alarm level |
200 mA |
||
Voltage Settings |
Undervoltage |
Trip enable |
Enable |
Trip level |
85 % |
||
Trip timeout |
3 s |
||
Alarm enable |
Enable |
||
Alarm level |
90 % |
Transfer the Configuration File
FLC (Full Load Current) Settings
FLC Basics
-
Load CT ratio = Load CT primary / (Load CT secondary * Passes)
-
Current sensor max = Current range max * Load CT ratio
-
Current range max is determined by the LTM R controller commercial reference. It is stored in units of 0.1 A and has one of the following values: 8.0, 27.0, or 100.0 A.
-
Contactor rating is stored in units of 0.1 A and is set by the user between 1.0 and 1000.0 A.
-
FLCmax is defined as the lower of the Current sensor max and the Contactor rating values.
-
FLCmin = Current sensor max / 20 (rounded to the nearest 0.01 A.). FLCmin is stored internally in units of 0.01 A.
Conversion of Amperes to FLC Settings
FLC values are stored as a percentage of FLCmax
FLC (in %) = FLC (in A) / FLCmax
Example (No External CTs)
Data:
-
FLC (in A) = 9 A
-
Current range max = 27.0 A
-
Load CT primary = 1
-
Load CT secondary = 1
-
Passes = 1or 2
-
Contactor rating = 18.0 A
Calculated parameters with 1 pass:
-
Load CT ratio = Load CT primary / (Load CT secondary * passes) = 1 / (1 * 1) = 1.0
-
Current sensor max = Current range max * Load CT ratio = 27.0 * 1.0 = 27.0 A
-
FLCmax = min (Current sensor max, Contactor rating) = min (27.0, 18.0) = 18.0 A
-
FLCmin = Current sensor max / 20 = 27.0 / 20 = 1.35 A
-
FLC (in %) = FLC (in A) / FLCmax = 9.0 / 18.0 = 50 %
Calculated parameters with 2 passes:
-
Load CT ratio = 1 / (1 * 2) = 0.5
-
Current sensor max = 27.0 * 0.5 = 13.5 A
-
FLCmax = min (13.5, 18.0) = 13.5 A
-
FLCmin = Current sensor max / 20 = 13.5 / 20 = 0.67 A
-
FLC (in %) = FLC (in A) / FLCmax = 9.0 / 13.5 = 66 %
Diagnostic
LTM R and LTM E LEDs
LEDs
Use the 5 LEDs on the face of the LTM R controller to monitor its state, as follows:
LTM R LEDs |
Color |
Describes |
Indicates |
---|---|---|---|
HMI Comm |
Yellow |
Communication activity between LTM R controller and LTM E expansion module |
|
Power |
Green |
LTM R controller power or internal trip condition |
|
Alarm |
Red |
Protection trip or alarm, or internal trip condition |
|
Fallback |
Red |
Communication connection between LTM R controller and network module |
|
MNS |
Yellow |
Communication activity on the network bus |
|
Use the 5 LEDs on the face of the LTM E expansion module to monitor its state:
LTM E LEDs |
Color |
Describes |
Indicates |
---|---|---|---|
Power |
Green or red |
Module power or internal trip condition |
|
Digital Inputs I.7, I.8, I.9 and I.10 |
Yellow |
State of input |
|
Use with TeSys T LTMCU Control Operator Unit
Available Functions
Once connected to the LTM R, the LTMCU can be used to:
-
configure parameters for the LTM R controller,
-
display information about the LTM R controller configuration and operation,
-
monitor trips and alarms generated by the controller,
-
control the motor locally using the local control interface.
LTM CU Front Face
Navigation Keys
The LTMCU navigation keys are contextual, that is, their function depends on the associated icons shown on the LCD display. These icons change for different displays, so the navigation key functions also change.
The navigation keys can be used to:
-
navigate menus and sub-menus,
-
scroll within a value list,
-
select a setting in a value list,
-
exit a value list without making a selection,
-
return to the main (first-level) menu,
-
switch between manual and automatic presentation mode in Quick View display.
The diagram below shows an example of the different functions of each of the navigation keys associated with an icon on the LCD display:

1 Information area of the LCD display
2 Contextual navigation icons area of the LCD display
3 Move up to the next higher-level menu
4 Move down to the next item in the menu
5 Select an item
6 Move up to the previous item in the menu
7 Return to the main menu
LCD Displays
The LTMCU presents 3 different LCD displays:
LCD display |
Functionality |
---|---|
Menu |
|
Quick View |
|
Detected Trips and Alarms |
|
Contextual Navigation Icons
The following table describes the icons used with the contextual navigation buttons on the LTMCU:
Icon |
Description |
Icon |
Description |
---|---|---|---|
Enables access to the main menu from a sub-menu or from Quick View |
Enables access to Quick View from the main menu or a sub-menu |
||
Scroll down |
Enables access to manual scroll mode (when Quick View is in automatic scroll mode) |
||
Scroll up |
Enables access to automatic scroll mode (when Quick View is in manual scroll mode) |
||
Validates a setting or value and enables access to a sub-menu when a menu is selected |
Used to increment a setting in menu mode |
||
Move up to the next higher-level menu |
Used to decrement a setting in menu mode |
||
When a menu item is password-protected, this icon enables access to the Enter Password screen |
Information Icons
The following table describes the icons provided as information in the information area of the LCD display. They indicate, among others, the selected menu or parameter:
Icon |
Description |
Icon |
Description |
---|---|---|---|
Main menu |
Indicates that the present display is Quick View |
||
Metering setting menu |
Indicates that a detected alarm has occurred |
||
Protection setting menu |
Indicates that a detected error has been detected |
||
Control setting menu |
Information |
||
Services menu |
Check box selected |
||
Language selection menu |
Check box unselected |
||
Radio button selected |
Item has been selected (for inclusion in Quick View display) |
||
Radio button unselected |
LTM R in Configuration mode |
Example of an HMI Display
Here is an example of HMI LCD displaying an average current of 0.39 A in local control, run mode:

1 Quick View display icon
2 Name of the setting currently displayed
3 Motor state
4 Short cut key to main menu
5 Manual scroll mode icon; pressing the associated contextual navigation key switches to manual scroll mode
6 Value of the setting currently displayed
Network Communication on DeviceNet™
Wire the Communication Port
Set the Parameters
For the application example, set the following parameters using SoMove™ software:
Settings Branch |
Sub-branch |
Parameter |
Setting |
---|---|---|---|
Device information |
– |
Network |
DeviceNet™ |
Communication |
Network port |
Address |
1 |
Baud Rate |
Autobaud |
||
Configuration via Network port |
Disabled |
You can set Baud Rate to Autobaud only if at least 1 secondary is configured with a specific Baud Rate.
Network Port Comm Loss parameter is enabled by default. If this is not suitable, you can disable this parameter.
Messaging
The connection types are:
-
I/O messaging
I/O messages contain application-specific data. They are communicated across single and multicast connections between an application producer and its corresponding consuming application.
-
Explicit messaging connections
Explicit messaging connections provide multipurpose point-to-point communication paths between two particular devices. Explicit messages are used to command the performance of a particular task and to report the results of performing the task. Use explicit messaging connections to configure nodes and diagnose conditions.
Communication Architecture

1 1756-A7 Allen-Bradley ControlLogix chassis with 7 slots
2 1756-PA72 Allen-Bradley ControlLogix power supply 120–240 Vac
3 1756-L71 Allen-Bradley ControlLogix controller, revision 24
4 1756-DNB Allen-Bradley ControlLogix DeviceNet™ scanner
5 LTMR27DFM LTM R controller communicating over DeviceNet™
6 LTMEV40FM LTM E Expansion module
7 Power tap
8 Power supply (24 Vdc)
Software Tools
Reference Number |
Freeware |
Description |
---|---|---|
9357-DNETL3 |
– |
RSNetWorx for DeviceNet™ application for configuring and monitoring DeviceNet™ networks and configuring connected devices. |
9324-RLD300ENE |
– |
RSLogix Designer configuring and programming software for the Allen-Bradley Logix5000 family of controller. |
– |
TeSys T MMC L |
A TeSys® T Motor Management Controller system without an expansion module, configurable via the HMI port. This variant enables you to preserve your local configuration. |
– |
TeSys T MMC L EV40 |
A TeSys® T Motor Management Controller system with expansion module, configurable via the HMI port. This variant enables you to preserve your local configuration. |
– |
TeSys T MMC R |
A TeSys® T Motor Management Controller system without expansion module configurable via the network. |
– |
TeSys T MMC R EV40 |
A TeSys® T Motor Management Controller system with expansion module configurable via the network. |
Assemble the Physical Network
To construct a physical DeviceNet™ network:
Step |
Action |
---|---|
1 |
Install the DeviceNet scanner module in the desired PLC slot. |
2 |
Check that the desired DeviceNet network node address and baud rate have been correctly set in SoMove. |
3 |
Make connections with DeviceNet™ network cable and end connectors, manufactured in accordance with ODVA specifications. |
4 |
Place the system on the network by connecting the PLC to the LTM R controller with the DeviceNet™ cable. |
5 |
Connect the RSNetWorx PC to the processor. |
Software Network Configuration
To configure the DeviceNet™ network:
Step |
Action |
Comment |
---|---|---|
1 |
Action in RSNetWorx. |
|
2 |
||
3 |
||
4 |
Action in Studio 5000. |
|
5 |
Register the Controller’s EDS
To register the controller’s EDS in RSNetWorx’s EDS library:
Step |
Action |
Result |
---|---|---|
1 |
From the menu, select . |
The wizard’s welcome screen appears. |
2 |
Click . |
The screen appears. |
3 |
Select and click . |
The screen appears. |
4 |
Select EDS file. and browse to the controller’sNOTE: You must have already unzipped the zip file containing
the EDS files and corresponding icons into
a single directory.
|
– |
5 |
Click . |
The screen appears. |
6 |
Click . |
screen appears. The controller should be listed in the field as a . |
7 |
Click . |
The screen appears. |
8 |
Verify that the controller is to be registered and click . |
The screen appears. |
Offline Controller Configuration
To add devices to your network when the configuration tool is offline:
Scanner Configuration
Step |
Action |
Result |
---|---|---|
1 |
From the view, double-click the scanner icon. |
The scanner configuration screen appears. |
2 |
Select the tab. |
The screen appears. |
3 |
At the MAC ID 1) in the list, and click the right arrow. tab, highlight the controller (at |
. |
4 |
With the controller selected, click the button. |
The window appears. |
5 |
Check and enter 8 in the text field and 6 in the text field.Click . |
|
6 |
Click . |
The window appears. |
7 |
Click . |
Wait for the timer to finish. |
8 |
Click . |
The scanner properties window closes. |
9 |
Click and select the project path.Click to save the global configuration to the PC. |
The global configuration can be saved only offline. |
PLC Configuration in Studio 5000
Step |
Action |
Result |
---|---|---|
1 |
In Studio 5000, select . |
– |
2 |
Select the type of controller. |
|
3 |
Select the chassis. |
|
4 |
Select . Right-click and select |
|
5 |
Select the Scanner in the list . |
|
6 |
The module properties appear. Select the input/output sizes in word:
Select the slot in the . Slot 4 in our example.Click to close the configuration. |
|
7 |
Select . Click the appropriate path and select . |
|
8 |
Download the application to the controller. |
– |
9 |
Select to run the scanner, then set . |
|
10 |
Select TeSys T. to see the data being returned from |
DeviceNet Communication Test
Registers for Simplified Operation
Command Variables 700-704
Instance 100: LTM R Control Registers:
Byte 0 |
Byte 1 |
Byte 2 |
Byte 3 |
Byte 4 |
Byte 5 |
---|---|---|---|---|---|
path 6C : 01 : 05 (Register 704) |
path 6C : 01 : 04 (Register 703) |
path 6C : 01 : 01 (Register 700) |
|||
LSB (least significant bit) |
MSB (most significant bit) |
LSB |
MSB |
LSB |
MSB |
Command variables 700-704 are described below:
Register |
DeviceNet Address |
Variable Type |
Read / Write Variables |
---|---|---|---|
700 |
6C : 01 : 01 |
Word |
Register available to remotely write commands that can be processed in a specific custom logic |
701-703 |
6C : 01 : 02 - 6C : 01 : 04 |
(Reserved) |
|
704 |
6C : 01 : 05 |
Word |
Control register 1 |
bit 0 Motor run forward command (1) |
|||
bit 1 Motor run reverse command (1) |
|||
bit 2 (Reserved) |
|||
bit 3 Trip reset command |
|||
bit 4 (Reserved) |
|||
bit 5 Self test command |
|||
bit 6 Motor low speed command |
|||
bits 7-15 (Reserved) |
|||
(1) Even in Overload mode, bits 0 and 1 of register 704 can be used to remotely control LO1 and LO2. |
Monitoring Variables 451, 455, 460, 466
Instance 110: LTM R Monitoring Registers (with dynamic configuration)
This assembly contains several monitoring registers commonly used with an LTM R device. You can choose registers by setting attributes 5-8 of the DeviceNet interface object:
Byte 0 |
Byte 1 |
Byte 2 |
Byte 3 |
Byte 4 |
Byte 5 |
Byte 6 |
Byte 7 |
---|---|---|---|---|---|---|---|
Register pointed using path C6 : 01 : 05 (Register 455) |
Register pointed using path C6: 01 : 06 (Register 460) |
Register pointed using path C6 : 01 : 07 (Register 451) |
Register pointed using path C6 : 01 : 08 (Register 466) |
||||
LSB |
MSB |
LSB |
MSB |
LSB |
MSB |
LSB |
MSB |
Monitoring variables 451, 455, 460, and 466 are described below:
Register |
DeviceNet Address |
Variable Type |
Read-only Variables |
---|---|---|---|
451 |
68 : 01 : 02 |
Ulnt |
Trip code (code of the last trip, or of the trip that takes priority) |
455 |
68 : 01 : 06 |
Word |
System status register 1 |
bit 0 System ready |
|||
bit 1 System on |
|||
bit 2 System trip |
|||
bit 3 System alarm |
|||
bit 4 System tripped |
|||
bit 5 Trip reset authorized |
|||
bit 6 Controller power |
|||
bit 7 Motor running (with detection of a current, if greater than 10% FLC) |
|||
bits 8-13 Motor average current ratio 32 = 100 % FLC - 63 = 200 % FLC |
|||
bit 14 In remote |
|||
bit 15 Motor starting (start in progress) 0 = descending current is less than 150 % FLC 1 = ascending current is greater than 10 % FLC |
|||
460 |
68 : 01 : 0B |
UInt |
Alarm code |
466 |
68 : 01 : 11 |
UInt |
Average current ratio (% FLC) |
This table will be updated later. Pierre to provide the changes.