DOCA0233EN-00

LTMTCUF Firmware Upgrade Using TeSys Programmer Tool

Overview

The firmware of the LTMTCUF control operator unit can be updated by using the TeSys Programmer Tool version 3.2.000 and above.

This chapter describes how to upgrade or downgrade the TeSys Tera LTMTCUF firmware. It explains how to prepare the LTMTCUF control operator unit and the PC, how to connect them, and how to start the TeSys Programmer Tool.

The latest LTMTCUF firmware version is LTMTCUF_HW2_V002.000.000_TERA.bin.

Setup

The following procedure describes how to establish physical link between the PC and the LTMTCUF control operator unit, and from the LTMTCUF control operator unit to the LTMT main unit:

  1. Power on LTMT main unit from a separate, externally supplied control power source that is switched from outside the enclosure.

  2. Connect the USB/RJ45 cable from a USB port of the PC, to the RJ45 connector port on the front face of the LTMTCUF control operator unit.

  3. Connect the free end of the LTMT9CU10S cable to the HMI port on the left side of the LTMT main unit.

    NOTE: It is recommended to make a direct link between the LTMT main unit and LTMTCUF control operator unit with the LTMT9CU10S cable.

  4. Route the cables to the outside of the enclosure to perform the update without exposure to energized equipment (doors closed and interlocked).

  5. Use a separate externally supplied control power source that is switched from outside of the enclosure, for the power connection. The control voltage supply must match the LTMT main unit input voltage.

    NOTE: Before proceeding, make sure that the power is OFF.

Firmware Upgrade

The programmer tool can be used for upgrading and downgrading firmware from the system.

  1. Download TeSys Programmer Tool from Schneider Electric Firmware Upgrade Tools.

  2. Run the TeSysProgTool.exe file.

    A pop-up safety message is displayed.

  3. Click Proceed to launch the Programmer.

    You can click Cancel to exit the Programmer.
  4. From the home screen, click LTMTCUF Upgrade on the top left corner of the screen.

  5. In the Firmware Package Selection field, click Browse, and navigate to the bin file.

  6. Select the LTMTCUF_HW2_V002.000.000_TERA.bin file of the latest LTMTCUF firmware. The firmware version will appear in the LTMTCUF Firmware Version field.

    NOTE: You must select the downloaded path TeSys Tera Firmware HMI file instead of the default TeSys Firmware HMI file.
  7. Make sure that there is proper connection between PC and LTMTCUF control operator unit, refer to Setup.

  8. In the Connectivity Settings field, select HW2 version.

    NOTE: The Programmer tool with LTMCU is applicable to LTMTCUF also.
  9. From the Select Serial Port drop-down, select the corresponding communication port and click Connect.

  10. The Connection Information pop-up message is displayed. Press both the STOP and RESET buttons on the LTMTCUF control operator unit, while powering on the LTMTCUF control operator unit with the LTMT main unit. Then press OK.

    NOTE: When properly connected, an hourglass will appear on the screen of the LTMTCUF control operator unit.

  11. In the Update LTMTCUF filed, click Update.

    IMPORTANT: Once the firmware update is in progress, do not disconnect the LTMTCUF control operator unit to avoid potential hardware corruption.
  12. Once the update is completed, Update OK pop-up message will appear. Click OK .

  13. Click Disconnect in the Connect PC to LTMTCUF filed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?