DOCA0233EN-00

Login Modes

User Mode

User mode allows monitoring and view settings (read only). Configuration of device and commands are restricted in user mode.

The top right corner of the setting screens will appear blank, and the OK icon will not be displayed on the setting screens.

Admin Mode

Admin mode allows complete access (read /write) to configuration settings and commands.

The top right corner of the setting screens will display the icon to denote that the LTMTCUF control operator unit is in configuration mode, and the OK icon will be displayed on the setting screens.

Login Procedure

The following table describes the procedure to log in as User or Admin:

Step

Description

Screen display

1

Go to Quick View mode.

2

Press OK, the login modes are displayed.

3

  • Select User and press OK. You are logged in as a user. The main menu is displayed.

  • Select Admin and press OK. Enter Pin screen is displayed

    .

4

Enter the six digits of the pin. The way to enter the pin is the same as for modifying the pin:

  • If the pin is correct, the main menu is displayed.

  • If the pin is incorrect, Incorrect pin! pop-up message is displayed before switching to Quick View.

Pin Setting Procedure

The LTMTCUF control operator unit has no pin set by default.

After the first LTMTCUF power up, the Set Pin screen is displayed to force the pin setting. The procedure to set the pin for the first time is described in the following table, from step 4.

Once the pin is set, it can be changed in the Settings menu. The modification of the pin is allowed in Admin mode. The following table describes the procedure to change the pin.

Step

Description

Screen display

1

Select Settings from the main menu. Press OK to enter the Settings menu.

2

Select the Display Setting sub-menu and press OK to enter.

3

Select Pin Change from the Display Setting sub-menu and press OK to enter.

4

The Set Pin screen is displayed, with the first digit of the pin highlighted.

  • Enter the first digit (0-9) of the new pin by using + and .

  • Press: the first digit is saved and the second digit is highlighted.

  • Enter the other digits in the same way.

  • Press OK when the last digit is set, to save the new pin.

5

The Confirm Pin screen is displayed. Enter the new pin as in the Set Pin screen and press OK.

6

  • If both the pins are identical, the Pin Set! pop-up message is displayed, to confirm the new pin is set.

  • If both the pins are not identical, the Incorrect Pin! pop-up message is displayed.

Forgotten Pin

If the pin is forgotten, it can be reset from the LTMT main unit by giving factory reset command.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?