DOCA0233EN-00

LTMTCUF Language Files Upgrade Using TeSys Programmer Tool

Overview

The language files of the LTMTCUF control operator unit can be updated by using the TeSys Programmer Tool version 3.2.000 and above.

The language file must be compatible with the LTMTCUF firmware version.

Language Files Upgrade

The programmer tool can be used for upgrading language files from the system.

  1. Download TeSys Programmer Tool from Schneider Electric Firmware Upgrade Tools.

  2. Run the TeSysProgTool.exe file.

    A pop-up safety message is displayed.

  3. Click Proceed to launch the Programmer.

    You can click Cancel to exit the Programmer.
  4. From the home screen, click LTMTCUF Language.

  5. In the Language Package Selection field, click Browse, and navigate to the LTMTCUF language folder.

  6. Select the LTMTCUF Language folder. The folder contains the following files:

    • Zipped folder of all languages (.zip)

    • Signature file (.sig)

  7. In the LTMTCUF Language version drop-down list, select LTMTCUF Languages_8075.

    NOTE: You must select the downloaded path TeSys Tera HMI language file instead of the default TeSys Tera HMI file.

    For more information, refer to Language Selection under First Setup Menu

  8. Select the required languages from the drop-down list.

    NOTE: By default, Language #1 is English, while Language #2 and Language #3 can be set as per the requirement.
  9. Make sure that there is proper connection between PC and LTMTCUF control operator unit, refer to Setup.

  10. In the Connectivity Settings field, select the corresponding communication port from the Select Serial Port drop-down. Click Connect.

  11. Once connected, the available language and version is displayed in the Connection Device Information.

  12. In the Update LTMTCUF field, click Update.

    IMPORTANT: Once the language update is in progress, do not disconnect the LTMTCUF control operator unit to avoid potential hardware corruption.
  13. Once the update is completed, Update OK pop-up message will appear. Click OK .

  14. Click Disconnect in the Connect PC to LTMTCUF field.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?