LTMT HMI Port Settings
The LTMT HMI port has the following configurable settings:
Setting | Setting range | Default setting |
---|---|---|
Node address | 1-247 in step of 1 | 1 |
Parity |
|
Even |
Baud rate |
|
19200 bps |
Endianness |
|
Big-endian |
-
Node address: 1
-
Baud rate: 19200 bps
NOTE: If baud rate is changed device will disconnected. -
Parity: Even
-
Endianness: Big-endian
The LTMT HMI port settings can be configured using the following interfaces:
-
A PC running the TeSys Tera DTM embedded in a FDT container, such as SoMove software.
-
A PLC or DCS via the communication protocol.