DOCA0233EN-00

HMI Display Modes

Overview

The LTMTCUF control operator unit supports the following display modes:

  • Quick View mode to display a selection of data.

  • Menu navigation mode to access all data through a menu structure.

When a trip is detected by the LTMT main unit, a Trip pop-up message appears and overrides the Quick View or Menu screen.

Quick View Mode

Quick View is the default HMI display mode. It displays a selection of data screens.

Menu Navigation Mode

In Menu navigation display mode, use the contextual buttons to navigate in the menu structure. Menu navigation display mode presents a single network of menus, with monitoring values and editable configuration settings.

Menu navigation is always accessible from Quick View screens by pressing the home button.

For more information on:

Trip Pop-Up Message

When a trip is detected by the LTMT main unit, a Trip pop-up message appears with the indication of the detected trip.

Press OK to acknowledge the Trip pop-up message. After acknowledgement of the Trip pop-up message, the LTMTCUF control operator unit falls back in the display mode active before the trip, Quick View or Menu navigation mode.

The trip data are available in the trip records. For more information, refer to trip records.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?