DOCA0278EN-00

Functionality Difference Between TeSys T System and TeSys Tera System

Added in Draft4

This section provides information about the functionality difference between TeSys T system and TeSys Tera system.

  • In the TeSys T system, only I3 input can be configured as an interlock, whereas in the TeSys Tera system, any input can be configured as an interlock.

  • In the TeSys T system, the reference voltage between common and digital input is depends on module reference (LTMRXFM is 230 Vac and LTMRXBD is 24 Vdc), whereas in the TeSys Tera system the reference digital input voltage is 24 Vdc.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.