DOCA0278EN-00

Equivalent Data Addresses

Overview

This chapter provides information about the equivalent data addresses to be used for performing the required functions after replacing the TeSys T system with the TeSys Tera system.

The equivalent data addresses are categorized into three sections as listed below:

  • Data addresses similar between TeSys T and TeSys Tera

  • Data addresses dissimilar between TeSys T and TeSys Tera

  • Data addresses not available in TeSys Tera

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.