TeSys T to TeSys Tera Commercial References
Equivalent Commercial References
The TeSys T system has the maximum capacity of equipping the LTMR controller with one LTME expansion module at a time. Whereas, the TeSys Tera system has the maximum capacity of equipping the LTMT main unit with one LTMTCT/LTMTCTV sensor module and up to five LTMT expansion modules.
The following protocols are supported by the TeSys Tera system for migration from TeSys T system:
-
Modbus RTU
-
PROFIBUS DP
-
EtherNet/IP
-
Modbus TCP/IP
The following protocols are not supported by the TeSys Tera system and cannot be migrated from TeSys T system:
-
CANopen
-
DeviceNet
The following table contains equivalent commercial reference numbers and combinations of the LTMT main unit and LTMT expansion modules that are suitable for replacing the TeSys T system:
| TeSys T |
TeSys Tera |
||
|---|---|---|---|
|
Main Controller |
Main Unit |
Sensor Module |
Expansion Unit 1 |
|
LTMR08MBD |
LTMTMBD |
Refer to the table below for the suitable LTMTCT/LTMTCTV sensor module to be added with the LTMT main unit. |
LTMTIN42BD |
|
LTMR08MFM |
LTMTMFM |
LTMTIN42FM |
|
|
LTMR08PBD |
LTMTPBD |
LTMTIN42BD |
|
|
LTMR08PFM |
LTMTPFM |
LTMTIN42FM |
|
|
LTMR08EBD |
LTMTEBD |
LTMTIN42BD |
|
|
LTMR08EFM |
LTMTEFM |
LTMTIN42FM |
|
|
LTMR27MBD |
LTMTMBD |
LTMTIN42BD |
|
|
LTMR27MFM |
LTMTMFM |
LTMTIN42FM |
|
|
LTMR27PBD |
LTMTPBD |
LTMTIN42BD |
|
|
LTMR27PFM |
LTMTPFM |
LTMTIN42FM |
|
|
LTMR27EBD |
LTMTEBD |
LTMTIN42BD |
|
|
LTMR27EFM |
LTMTEFM |
LTMTIN42FM |
|
|
LTMR100MBD |
LTMTMBD |
LTMTIN42BD |
|
|
LTMR100MFM |
LTMTMFM |
LTMTIN42FM |
|
|
LTMR100PBD |
LTMTPBD |
LTMTIN42BD |
|
|
LTMR100PFM |
LTMTPFM |
LTMTIN42FM |
|
|
LTMR100EBD |
LTMTEBD |
LTMTIN42BD |
|
|
LTMR100EFM |
LTMTEFM |
LTMTIN42FM |
|
| TeSys T |
TeSys Tera |
||||
|---|---|---|---|---|---|
|
Main Controller |
Expansion Module |
Main Unit |
Sensor Module |
Expansion Unit 1 |
Expansion Unit 2 |
|
LTMR08MBD |
LTMEV40BD |
LTMTMBD |
Refer to the table below for the suitable LTMTCT/LTMTCTV sensor module to be added with the LTMT main unit. |
LTMTIN42BD |
LTMTIN42BD |
|
LTMR08MFM |
LTMEV40FM |
LTMTMFM |
LTMTIN42FM |
LTMTIN42FM |
|
|
LTMR08PBD |
LTMEV40BD |
LTMTPBD |
LTMTIN42BD |
LTMTIN42BD |
|
|
LTMR08PFM |
LTMEV40FM |
LTMTPFM |
LTMTIN42FM |
LTMTIN42FM |
|
|
LTMR08EBD |
LTMEV40BD |
LTMTEBD |
LTMTIN42BD |
LTMTIN42BD |
|
|
LTMR08EFM |
LTMEV40FM |
LTMTEFM |
LTMTIN42FM |
LTMTIN42FM |
|
|
LTMR27MBD |
LTMEV40BD |
LTMTMBD |
LTMTIN42BD |
LTMTIN42BD |
|
|
LTMR27MFM |
LTMEV40FM |
LTMTMFM |
LTMTIN42FM |
LTMTIN42FM |
|
|
LTMR27PBD |
LTMEV40BD |
LTMTPBD |
LTMTIN42BD |
LTMTIN42BD |
|
|
LTMR27PFM |
LTMEV40FM |
LTMTPFM |
LTMTIN42FM |
LTMTIN42FM |
|
|
LTMR27EBD |
LTMEV40BD |
LTMTEBD |
LTMTIN42BD |
LTMTIN42BD |
|
|
LTMR27EFM |
LTMEV40FM |
LTMTEFM |
LTMTIN42FM |
LTMTIN42FM |
|
|
LTMR100MBD |
LTMEV40BD |
LTMTMBD |
LTMTIN42BD |
LTMTIN42BD |
|
|
LTMR100MFM |
LTMEV40FM |
LTMTMFM |
LTMTIN42FM |
LTMTIN42FM |
|
|
LTMR100PBD |
LTMEV40BD |
LTMTPBD |
LTMTIN42BD |
LTMTIN42BD |
|
|
LTMR100PFM |
LTMEV40FM |
LTMTPFM |
LTMTIN42FM |
LTMTIN42FM |
|
|
LTMR100EBD |
LTMEV40BD |
LTMTEBD |
LTMTIN42BD |
LTMTIN42BD |
|
|
LTMR100EFM |
LTMEV40FM |
LTMTEFM |
LTMTIN42FM |
LTMTIN42FM |
|
LTMTCT/LTMTCTV Sensor Modules
The following table contains commercial reference numbers and combinations of the LTMTCT/LTMTCTV sensor modules, which are suitable for replacing the TeSys T system:
|
Motor Full Load Current Value |
Reference |
|---|---|
|
0.3 to 3 A |
LTMTCT3T |
|
LTMTCTV3T |
|
|
LTMTCTV3UT |
|
|
2.5 to 25 A |
LTMTCT25T |
|
LTMTCTV25T |
|
|
LTMTCTV25UT |
|
|
10 to 100 A |
LTMTCT100T |
|
LTMTCTV100T |
|
|
LTMTCTV100UT |