8800DB0101R05/24

Introduction

This document is a supplement to Schneider Electric Conditions of Sale, Standard (publication number 0100PL0041). It provides additional information on warranties, returns, and exchanges for all drives and soft starters available from Schneider Electric and authorized sales channels.

Product Offer

Current soft starter and adjustable speed drive offers are listed in the following table. Refer to the Digest or Altivardrives.com for additional information on Schneider Electric drive and soft starter products.

Soft Starter and Adjustable Speed Drives Offer

Soft Starters

Altivar 480 Legacy Soft Starters Altivar 48
Altistart 01
Altistart 22

Adjustable Speed Drives

Altivar 12

Legacy Drives Altivar 312

Altivar 212

Altivar 61

Altivar 320

Altivar 71

Altivar 340

Altivar 66

Altivar 630

Altivar 58

Altivar 650

Altivar 930

Altivar 950
Altivar 660
Altivar 960
Altivar 680
Altivar Outdoor 630
Altivar Outdoor 930
Customer Low Voltage Drives
Altivar Process Modules (APM)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.