DUG_FUGA Rotary Dimmer_LK-01

About the device

LK FUGA® Wiser Multiwire LED Rotary Dimmer (hereinafter referred to as Rotary Dimmer), you can switch and dim LED lamps, ohmic, inductive or capacitive loads.

Control options

Home control: To control the dimmer through the Wiser app you will need the Wiser Gateway.

Functions:

  • Automatic load detection

  • Thermal protection, overload-resistant, short-circuit protection, soft start, soft stop

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?