DUG_FUGA Rotary Dimmer_LK-01

Creating a schedule

The Rotary Dimmer can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.
  1. On the Home page, tap All devices > Rotary Dimmer.
  2. Tap Schedule > Add schedule to add a schedule.
  3. Set the time (A).
  4. Tap Repeat (B) to select the days you want to set the schedule.
  5. Tap Note (C), enter the note and tap Confirm.
  6. Tap the toggle switch to turn on the Notification (D) for the schedule. The app will send a notification that the scheduled task is executed at the time of schedule.
  7. Adjust the Brightness settings (E) through sliding bar.

  8. Tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?