DUG_FUGA Rotary Dimmer_LK-01

Example of an automation

This demonstration shows you how to create an automation to switch On the light when a window door sensor is activated at night.
NOTE: The Dimmer will not be switched Off automatically when the sensor sends the "Closed" message. To switch Off the dimmer when the door is closed, you must create a new automation.
  1. Go to Automation > + icon to create an automation.
  2. Tap Edit name , enter the name of the automation and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping icon.
  3. Tap Add Condition > When device status changes > Window Door Sensor.
  4. Tap Window Door Sensor > Open (A).
  5. Tap Add task > Run the device > Rotary Dimmer.
  6. Tap Rotary Dimmer (B) and tap On in the slide-up menu.
  7. Tap Effective period, select Night and tap Next.
  8. In the Automation Settings page, tap Save.
    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?