DUG_FUGA Rotary Dimmer_LK-01

Switching/Dimming the device using app

Using the Wiser app, you can turn on/off and increase/decrease the brightness of the device.

Switch On/Off the device

Follow the steps to turn on/off the device:

  1. On the Home page, tap the power button (A) to turn on/off the dimmer.

  2. Alternatively, you can navigate to the control panel of the device and tap to turn on/off the dimmer.

    NOTE: The control panel shows the current state of the Dimmer.

Adjusting the brightness of the device

Follow the steps to increase/decrease the brightness of the device:

  1. On the Home page, tap the ˅ and drag the slider to adjust the brightness of the Dimmer.

  2. Alternatively, you can navigate to the control panel of the device and drag the sliding bar up/down to increase/decrease the brightness.

    NOTE: The control panel shows the current brightness percentage of the Dimmer.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?