DUG_PowerTag-E_LK-03

Adding tariff rate

You can add flat and peak rate value in the Wiser app.
  1. Tap Add a Rate on Electricity page.
  2. Enter name and rate per kWh (A).
  3. Tap Add (B).

    TIP: You can set the highest tariff rate as a peak rate and other tariff rates as an off-peak rate.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?