DUG_PowerTag-E_LK-03

Example of an Automation

This demonstration shows you how to create an automation to switch off the load and receive notification when total active power consumption is more than set value.
  1. Go to Automation > + to create an automation.
  2. Tap , enter the name of the automation and tap Save.
    TIP: You can choose the cover image that best represents your automation by tapping .
  3. Tap Add Condition > When device status changes > Grid > Total Active Power.
  4. Enter a target value (A), tap > (B) and then tap Next.
  5. Tap Add task > Run the device > Light.
  6. On Select function window, tap Switch from the slide-up menu and select Off > Save > Next.
  7. Tap Add task > Send Notification select Notification then tap Next.
  8. In the Automation Settings page, tap Save.
    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?