DUG_PowerTag-E_LK-03

Pairing device manually

To pair the device manually:
  1. On the Home page, tap +.
  2. Tap , select the required Wiser Hub on the slide-up menu.
  3. Select an option to add the device (A):
    • Add Device with Install Code
    • Add Device without Install Code

    TIP: It is recommended to add the device with install code.
  4. To pair the device with install code, tap Add Device with Install Code to display the slide-up menu. Select any one of the options (B):
    • Scan Install Code: you can scan the device for the install code.

      Position your camera to scan the QR code or barcode available on the PowerTag.

    • Enter Install Code Manually: you can manually enter the install code on the device.

    After adding the device with Install Code, proceed to Step 6.
  5. To pair the device without install code, tap Add Device without Install Code.
  6. Select Confirm LED is blinking amber > Start Configuration (C).

    NOTE: PowerTag must be connected to the MCB and powered ON.

  7. Wait for a few minutes for the app to connect with your PowerTag.
    Once PowerTag is added, tap Done.
  8. On the configuration page, tap on the PowerTag to configure.
  9. Tap Upgrade, to update to the latest version and unlock the respective features.
    NOTE: By default, the first two steps will be completed for new users.

  10. Once all upgrade steps are completed, you will get a pop-up notification. Tap Confirm, to open settings page.
  11. On the settings page, tap (D) to select the type.
  12. Select the type from the list based on the usage and appliance, then tap Confirm.
    IMPORTANT: It is mandatory to configure a PowerTag as Grid on the main incomer of the house.
  13. Tap Name (E), enter the name then tap Save.
    TIP: You cannot add the same name twice, and use the name Grid.
    By default name will be taken from the type selected.
  14. On setting page, tap Save > Confirm > OK.on pop-up notification.
    NOTE: Once you configure, you will not be able to change the load type you are monitoring.
    To monitor another load type in the future, you have to remove and re-configure the PowerTag.
  15. Once all PowerTag are configured, tap Done.

    On successful pairing, PowerTag will appear on the home screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?