DUG_PowerTag-E_LK-03

Pairing the device

Pair your PowerTag with the Gateway/Hub to access and control the PowerTag using the Wiser app.
  • We recommend to configure your main PowerTag as Grid on the main incomer of the house. This helps to record the overall consumption.

    NOTE:
    • Grid: main supply (referred as Grid in the app) of the house.

    • Load: power consumed from the Grid or a production source by electrical devices such as light, water heater, and fridge.

  • If you have more than one PowerTag installed, it is recommended to pair the main PowerTag first and set it as Grid.

    NOTE:
    • Main PowerTag is connected to the Grid.

    • Additional PowerTag are connected to the loads.

IMPORTANT: PowerTag must be installed by qualified professional.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?