DUG_PowerTag-E_LK-03

About the device

PowerTag E (hereinafter referred as PowerTag) is a compact, robust, and easy-to-install wireless communication energy sensor. It is used together with the Gateway/Hub to collect information from every equipped circuit to identify the energy consumption of each connected load. It is designed specifically to manage energy consumption for new and existing residential installations. It monitors and measures energy and power in real-time, and also provides complete visibility of power transfer between power source and loads.

Features of PowerTag:

  • Easily mounted with top or bottom position directly on circuit breaker.

  • Measures energy consumption and real-time power.

  • Sends real-time notifications and alarms to the Wiser app in case of consumption limit set by user in automation exceeds.

Benefits of PowerTag:

  • Easy accessibility and fastest installation.

  • Energy Class 1: accurate measurement.

  • Compact and cost effective.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?