DUG_Smoke Alarm-Battery_LK-01

For your safety

NOTICE
EQUIPMENT INSTALLATION HAZARD
  • Always operate the product in compliance with the specified technical data.
  • Keep the installation instruction for the life of the product.
Failure to follow these instructions can result in equipment damage.
WARNING
SEALED BATTERY HAZARD
Do not recharge, disassemble or incinerate the battery.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?