DUG_Smoke Alarm-Battery_LK-01

Testing the interconnected device(s)

It is possible to test all the devices simultaneously in an interconnected network with one operation.
  1. Select any interconnected device.
  2. Press and hold the Test/Hush button for more than 10 s until an alarm goes off on all interconnected devices.

  3. If there is no alarm triggered on the interconnected devices, check if the distance between each device is within the specification. Also check that the device is On and working properly. Refer troubleshooting smoke alarm battery.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?