DUG_Smoke Alarm-Battery_LK-01

Pairing device manually

To pair devices manually:
  1. Locate the power switch on the rear side of the device. Use a screwdriver to turn the power switch to ON position.

    NOTE: When mounted on wall or the ceiling, the device is automatically turned ON.
  2. In Wiser app Home page, tap +.
  3. Tap and select the required Wiser Hub on the slide-up menu.
  4. Select any one of the options to add device (A):
    • Add Device with Install Code
    • Add Device without Install Code

  5. To pair the device with an install code,, tap Add Device with Install Code to display the slide-up menu. Select any one of the options (B):
    • Scan Install Code - You can scan the device for the an install code.
    • Enter Install Code Manually - You can manually enter the install code from the device
    After pairing the device with an install code, proceed to Step 7.

    TIP: It is highly recommended to pair the device with Install code.
  6. To pair the device without install code, tap Add Device without Install Code.
  7. Once the device is On, press Set/Reset button 3 times.

    The LED blinks yellow.
  8. In the app, select LED is blinking yellow and tap Start Configuration (C).
  9. After a few seconds, a solid green LED indicates that the device has been successfully paired.

  10. Once the device is paired in the app, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?