DUG_Smoke Alarm-Battery_LK-01

Interconnecting devices without Wiser Gateway

The smoke alarms (devices) can be connected directly to each other via RF connections even without a Wiser Gateway/Hub network.

IMPORTANT: Turn the power switch to ON position on all the devices.
  1. Identify a device and mark it as Master with a label supplied. Other devices are considered as Slave.

  2. Short press the Test/Hush button 3 times within 2 s on the primary device.


    The Standby LED turns on for 30 s once it is in pairing mode.

  3. Identify a Slave device and short press the Test/Hush button 3 times within 2 s.


    The Standby LED blinks 3 times on both Master and devices indicating a successful RF connection. Than on the Master device, the Standby LED again turns on for 30 s

Repeat the step 3 on all Slave devices.

NOTE: To exit from pairing mode, short press (< 0,5 s) the Test/Hush button 3 times on the Master device. The Standby LED turns off indicating that the Master device is not in pairing mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?