DUG_Wiser wireless ceiling PIR_LK-00

Detection delay

Using the wiser app, you can set the detection delay time.
To set the detection delay duration:
  1. On the Home page, tap All devices > Motion Sensor.
  2. On the device control panel page, tap Settings.
  3. Short press the function key once or simulate the motion to wake up the device.
  4. Tap Detection Delay and select the time duration (A).
  5. Tap Detection Delay Customization (B) to customize your detection delay time. You can set the time between 00:01 to 59:59 minutes.
    NOTE:
    • Modifying the detection delay time to long-interval will affect the battery life of the sensor.

    • Each detected motion resets the delay time. Thus the delay time begins with the last motion detected.

    EXAMPLE: If you set the detection delay time to 5 minutes and there is a motion, the information "Occupied" will be sent to the Wiser gateway. If there is no motion detected in last 5 minutes (configured detection delay time), the information "Unoccupied" will be sent to the Gateway.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?