DUG_Wiser wireless ceiling PIR_LK-00

Pairing device manually

To pair the device manually:
  1. On Home page, tap +.
  2. Tap , select the required Wiser Hub on the slide-up menu.
  3. Select an option to add the device (A):
    • Add Device with Install Code
    • Add Device without Install Code

    TIP: It is highly recommended to add the device with install code.
  4. To pair the device with an install code, tap Add Device with Install Code to display the slide-up menu. Select any one of the options (B):
    • Scan Install Code - you can scan the device for the install code.
    • Enter Install Code Manually - you can manually enter the install code from the device.
    After pairing the device with install code, proceed to Step 6.

  5. To pair the device without install code, tap Add Device without Install Code.
  6. On the rear side of the sensor, short press (< 0,5 s) the function key 3 times.

    The LED blinks orange.
  7. In the app, select Confirm LED is flashing orange and tap Start configuration (C).
    The app displays the progress of connecting the device.
  8. After a few seconds, a solid green LED indicates that the sensor is successfully paired to the Gateway.

  9. Tap Done when the pairing is successful.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?