DUG_Wiser wireless ceiling PIR_LK-00

Example of an automation

This demonstration shows you how to create an automation to switch on the light with 50% brightness level when a motion is detected.
NOTE: The Dimmer will not be switched off automatically when the Sensor sends the "Unoccupied" message. To switch off the dimmer when there is no more motion, you must create a new automation.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name , enter the name of the automation and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping .
  3. Tap Add Condition > When device status changes > Motion Sensor.
  4. Tap Motion State > Occupied (A).

  5. Tap Add task > Run the device > .
  6. Tap Brightness (B), adjust the brightness to 50% and tap Save.
    TIP: Setting the brightness level turns on the light the light when the automation is triggered. You need not add a task to turn on the Dimmer separately.

  7. Tap Next.
  8. In the Automation Settings page, tap Save.
    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?