DUG_Wiser wireless ceiling PIR_LK-00

Creating an automation

An automation allows you to group multiple actions that are usually done together, triggered automatically or at scheduled times. By using the Wiser app, you can create automations based on your needs.
  1. On the Home page, tap the .
  2. Go to Automation > + to create an automation.
  3. Tap Edit name , enter the name of the automation (A) and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping .

  4. Tap Any condition is met to select any one of the condition type (B):
    • All conditions are met- The automation is triggered when all the conditions are met.
    • Any condition is met- The automation is triggered when at least one condition is met.

  5. Tap Add Condition to display the slide-up menu.
  6. In the Add Condition menu, you can do either or all of the following options (C):
    • When weather changes - Select various weather settings
    • Schedule - Set the time and day
    • When device status changes - Select the device and its function
    NOTE: You can add one or more conditions using .

  7. Tap When device status changes > Motion Sensor to select either or all of the functions to add in the automation:
    • Lux level - Select any level from Very dark to Very bright (D)
      NOTE: The value for Very dark to Bright can be set in the Lux Setting. The Very bright setting will take the maximum lux setting value (2000 lux).
    • Motion state - Occupied, if a motion is detected. Unoccupied, if there is no motion (E)
    • Current lux value - Select the condition (F) and the lux value (G)

  8. Tap Add task to display the slide-up menu.
  9. In the Add task menu, you can do either or all of the following options (H):
    • Run the device- Select the devices that you want to trigger.
    • Moment or Automation- Select the moment which you want to trigger or select the automation that you want to enable or disable.
    • Send notification- Turn on notification for the automation.
    • Delay - Set the delay time.
    NOTE: You can add one or more actions using icon.

  10. Tap on Effective period to set the time range for the automation. You can select any one of the following (I):
    • All-day - 24 hours
    • Daytime - From sunrise to sunset
    • Night - From sunset to sunrise
    • Custom - User defined time period

  11. Once all the actions and conditions are set, tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?