DUG_Wiser wireless ceiling PIR_LK-00

About the device

The Wiser Motion Sensor (hereinafter referred to as sensor) detects nearby movement and measures the luminance of the environment.

The sensor sends the data to the . The threshold of luminance settings and/or detection of movement can be configured in the Wiser app.

Features of the sensor:

  • Detect motion and send this information to the .

  • Detect and measure the lux level of the environment and passes the information to the .

  • Sends the sensor battery level and offline status information to the .

Operating elements

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?