DUG_Sedna Motion Sensor Dimmer_WSE-00

Creating a schedule

The Motion Sensor Dimmer can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.
  1. On the Home page, tap All devices > Motion Sensor Dimmer.
  2. Tap Schedule > Add schedule to add a schedule.
  3. Set the time (A).
  4. Tap Repeat (B) to select the days you want to set the schedule.
  5. Tap Note (C), enter the note and tap Confirm.
  6. Tap the toggle switch (D) to turn on the Notification for the schedule. The app will send a notification when the scheduled task is executed at the time of schedule.
  7. Adjust the Brightness settings (E) through sliding bar.
    • 100% - Turns on the dimmer with maximum brightness on the scheduled time
    • Off - Turns off the dimmer on the scheduled time

    Drag the sliding bar anywhere in between to turn on the dimmer with a set brightness level on the scheduled time.

  8. Tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?