DUG_Sedna Motion Sensor Dimmer_WSE-00

Resetting the device

You can reset the device to factory default manually.

Short press push button 3 times (< 0.5 s) and then long press the push button once (>10 s), LED starts blinking red then release the push button.
The LED stops blinking upon successful reset of the device. The Motion Sensor Dimmer restarts and blinks green for a few seconds.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?