DUG_Sedna Motion Sensor Dimmer_WSE-00

Example of an automation

This demonstration shows you how to create an automation to get notification on your app when the motion is detected.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name , enter the name of the automation and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping .
  3. Tap Add Condition > When device status changes > Motion Sensor Dimmer.
  4. In Select function menu tap on Motion State > Occupied (A).

  5. Tap Add task > Send Notification and select Notifications (B).

  6. Tap Next.
  7. In the Automation Settings page, tap Save.

    Automation is now available under Automation tab. Use toggle switch to enable/disable automation.
Push notification will appear on the screen when the automation is triggered. You can also tap on to access the notification history.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?