DUG_Sedna Motion Sensor Dimmer_WSE-00

Switching/Dimming the device using app

Using the Wiser app, you can turn on/off and increase/decrease the brightness of the device.
  1. On the Home page, tap the power button (A) to turn on/off the Motion Sensor Dimmer.

  2. In home page, next to device name, tap the ˅ for common function and drag the sliding bar (B) to adjust the brightness of the dimmer.

  3. Alternatively, you can navigate to the control panel of the device and tap to turn on/off the and use the sliding bar to adjust the brightness.
    NOTE: The control panel shows the current state of the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?