DUG_Sedna Motion Sensor Dimmer_WSE-00

Removing the device

Using the Wiser app, you can remove a device from the device list.
  1. On the Home page, tap All devices > Motion Sensor Dimmer.
  2. Tap to display more details.
  3. Tap Remove and Factory Reset Device (A).

    TIP: On the home page, you can tap and hold the Motion Sensor Dimmer to remove the device., you can long tap on the on the Home page to remove the device.
    NOTE: By removing the device, you will reset the device. If you still have a problem with the reset, then refer to resetting the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?