DUG_Sedna Push-button Dimmer_WSE-00

About the device

The Connected Multiwire Universal Push-button Dimmer LED (hereinafter referred to as Dimmer) is a push-button device that can be used to switch and dim LED, ohmic, inductive or capacitive loads manually or remotely. It can detect the load automatically and provides thermal protection, overload-resistance and short-circuit protection.

Control options

Home control: To control the dimmer through the Wiser app you will need the Wiser Gateway.

Direct operation: The dimmer can always be controlled directly on-site. You can also connect any number of mechanical push-buttons to control the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?