DUG_Sedna Push-button Dimmer_WSE-00

Switching/Dimming the device using app

Using the Wiser app, you can switch on/off and increase/decrease the brightness of the device.

Switch On/Off the device

  1. On the Home page, tap the power button (A) to switch on/off the Dimmer.

  2. Alternatively, you can navigate to the control panel of the device and tap to switch on/off the Dimmer.

    NOTE: The control panel shows the current state of the Dimmer.

Adjusting the brightness of the device

To increase/decrease the brightness of the device:

  1. In home page, next to device name, tap ˅ (B) for common function and drag the slider to adjust the brightness of the Dimmer.

  2. Alternatively. you can navigate to the control panel of the device and drag the sliding bar up/down to increase/decrease the brightness.

    NOTE: The control panel shows the current brightness percentage of the Dimmer.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?