DUG_Sedna Push-button Dimmer_WSE-00

Creating a moment

A Moment allows you to group multiple actions that are usually done together. Using the Wiser app, you can create moments based on your needs (such as movie night).
  1. On the Home page, tap .
  2. Go to Moment > + to create a moment.
  3. Tap Edit name , enter the name of the moment (A) and tap Save.
    TIP: You can choose the cover image that represents your moment by tapping .

  4. In the Action section, tap Add task (B) to display the slide-up menu.
  5. In the Add task menu, you can do either or all of the following actions (C):
    • Run the device: select the devices that you want in a moment.
    • Select Automation: select the automation that you want to enable or disable. For more info refer to Automation.
    • Delay: set the delay time.
    NOTE: You can add one or more actions using .

  6. Tap Run the device > Push-button Dimmer and select either or both the functions to add in the moment:
    • Dimmer: turn the Dimmer on/off (D).
    • Brightness: adjust the brightness level (E).
  7. Set all actions and tap Save.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?