DUG_Sedna Push-button Dimmer_WSE-00

Resetting the device

You can reset the device to factory default manually.

Short press push button 3 times (< 0.5 s) and then long press the push button once (>10 s). after 10 s, LED starts blinking red then release the push button.
The LED stops blinking upon successful reset of the device.
The Push-button Dimmer restarts and blinks green for a few seconds.

NOTE: After reset, the LED turns amber indicating that it is ready for pairing.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?