DUG_Motion sensor with dimmer_WSE-01

Switching/Dimming the device manually

You can switch On/Off and increase/decrease the brightness of the Dimmer manually. The Dimmer will provide power to the load connected to it.
Short press the push button on the device once to switch On/Off the Motion Sensor Dimmer.


Long press the push button on the device to increase/decrease the brightness of the Dimmer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?