DUG_Motion sensor with dimmer_WSE-01

About the device

The Connected Motion Sensor with Dimmer LED (hereinafter referred to as Motion sensor dimmer) detects moving heat sources (e.g. persons) and can dim ohmic, inductive or capacitive loads and switch them on for a settable overtravel time.

Control options

Home control: To control the motion sensor through the Wiser app you will need the Wiser Gateway.

Direct operation: The motion sensor can always be controlled directly on-site. You can also connect any number of mechanical push-buttons.

Functions

  • Detection range

  • Automatic load detection

  • Automatic mode, manual operation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?