DUG_Motion sensor with dimmer_WSE-01

Using the device

On the Home page, tap All devices > Motion Sensor Dimmer to access the control panel.

On the control panel page, you can see the following:

  • The motion detection and current Lux level (A)

  • The current device state and brightness level (B)

  • Sliding bar to adjust the brightness (C)

  • Schedule (D)

  • Settings (E)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?