DUG_Motion sensor with dimmer_WSE-01

Switching/Dimming the device using app

Using the Wiser app, you can switch On/Off and increase/decrease the brightness of the device.
To switch the device On/Off:
  1. On the Home page, tap the power button (A) to switch On/Off the Motion Sensor Dimmer.

  2. Tap the ˅ for common function and drag the slider (B) to adjust the brightness of the dimmer.

  3. Alternatively, you can navigate to the control panel of the device and tap to switch On/Off the and use the slider to adjust the brightness of Motion Sensor Dimmer.
    NOTE: The control panel shows the current state of the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?