DUG_Unica-Motion Sensor_WSE-01

Motion sensor switch settings

Using The Wiser app, you can manage the switch settings.

To access the motion sensor switch settings:

  1. On the Home page, tap All devices > Motion Sensor Switch.

  2. On the device control panel page, tap Settings.

Sensitivity Setting

Using the Wiser app, you can set the sensitivity of the sensor (such as High, Medium, Low).

Tap Sensitivity Setting and select one of the following levels (A):

  • High

  • Medium

  • Low

NOTE: The high sensitivity level detects the slightest movement.

Detection Delay

Using the wiser app, you can set the detection delay time.

Tap Detection Delay and select the time duration (B) or tap Detection delay custom (C) to customize your detection delay time.

Lux Customization

Using the Wiser app, you can define the threshold value for lux ranges (such as very dark, dark, bright, very bright) of the environment. This will prevent the false alarm caused by changes in the light intensity.

Tap Lux Threshold and drag the slider bar (D) to define its threshold value and tap Save.

  • Very dark level - Lux value ranges from 1 lux to 100 lux

  • Dark level - Lux level ranges from 6 lux to 300 lux

  • Bright level - Lux level ranges from 101 lux to 2000 lux

NOTE: The Current Lux Value is the current light level present in the environment measured by the sensor.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?