DUG_Unica-Motion Sensor_WSE-01

Using the device

The Control Panel allows you to switch the Motion Sensor Switch On and Off and control various settings.

On the Home page, tap All devices > Motion Sensor Switch to access the control panel.

On the control panel page, you can see the following:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?