DUG_Unica-Motion Sensor_WSE-01

Pairing device manually

To pair the device manually:
  1. On Home page, tap +.
  2. Tap and select the Wiser Hub.
  3. Select an option to add the device (A):
    • Add Device with Install Code
    • Add Device without Install Code

    TIP: It is highly recommended to add the device with install code.
  4. To pair the device with an install code, tap Add Device with Install Code to display the slide-up menu. Select any one of the options (B):
    • Scan Install Code - you can scan the device for the install code.
    • Enter Install Code Manually - you can manually enter the install code from the device.
    After pairing the device with install code, proceed to Step 6.

  5. To pair the device without Install Code, tap Add Device without Install Code.
  6. Short press the push button 3 times (< 0,5 s) on the device.

    The LED blinks amber.
  7. In the app, select Confirm LED is blinking amber and tap Start configuration (C).

  8. After a few seconds, a solid green LED indicates that the device has been successfully paired to the Gateway/Hub.

  9. Tap Done when the pairing is successful.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?