DUG_LK Fuga Push-button Switch_WH-00

About the device

The LK FUGA® Wiser Push-button Switch (hereinafter referred to as relay switch) is a push button device that can be used to switch LED, ohmic, inductive or capacitive loads manually or remotely.

Control options

Home control: To control the relay switch through the Wiser Home app you will need the Wiser Hub.

Direct operation: The relay switch can always be controlled directly on-site. You can also connect any number of mechanical push-buttons.

Room control / Quick Home Connect: The relay switch can operate without the Wiser Hub or a smartphone application.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?