DUG_LK Fuga Push-button Switch_WH-00

Configuring the device

The Device Details screen allows you to configure the device settings according to your preferences.
  1. On the Home screen, tap .
  2. Tap Devices > Lights > Relay switch to locate to the Device Details screen.
    TIP: You can also navigate by tapping Control > Select the device > > Device Settings.

    A

    Device Name: Tap to change the name of the device.

    B

    Location: Tap to assign the Device to any room (such as living room, bedroom, kitchen etc). For more information, refer to Setting the device location.

    C

    LED Indicator Behaviour: Tap to set the LED indicator behaviour of the device as per your preference. Refer to Setting up the LED Indicator Behaviour for detailed information on each option.

    D

    Identify: Tap to identify the device. The status LED blinks red and connected lighting devices blinks on/off, upon successful identification of the switch.
    Tap OK when you finish identifying the device.

    E

    Delete: Tap to remove the device from the system.

    NOTE:
    • Removing the device will also reset the switch. After reset, the LED turns amber indicating that the switch is ready for pairing.

    • If there is a problem while pairing or resetting the switch, refer to Resetting the device.

    F

    Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator which displays the current signal strength of the device.

    • Good Signal (between 0 & -54dBm)

    • Normal Signal (between -54 & -79dBm)

    • Poor Signal (<-79dBm)

    • No Signal (device is offline)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?